This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Amplifier Design for Headphone Driver

Prodigy 40 points

Replies: 7

Views: 609

Hi
If we would like to use amplifier design for headphone driver, any recommend amplifier part number?
Thank you.

Vader
  • Hi Vader,

    I would recommend you take a look at the TI.com selection tools for op-amps. It is difficult to know what to recommend without more information on your application. 

    http://www.ti.com/amplifier-circuit/op-amps/overview.html

    There are also TI designs such as this one which might help guide you as well.

    http://www.ti.com/tool/TIPD189 

    Hope that helps,

    Paul

  • In reply to Paul Goedeke:

    Hi Sir,
    I would like to know the root cause of Vp-p is too small come from
    1. component's value choose wrong
    2. OP AMP IC solution choose wrong(HP design need specify OP AMP)
    3. design structure choose wrong(for example to change non-inverting to inverting....)

    Thank you.

    Vader
  • In reply to Vader chen:

    Hi Vader,

    as I already mentioned above: The OPA172 cannot drive a 32R load! If you decrease R70 to 0R then the maximum output voltage is about 2Vpp. Is this enough for your application? A higher output level is not possible with the OPA172.

    If you need a higher output level, then you must choose a headphone amplifier.

    Kai
  • In reply to kai klaas69:

    Hi Kai,
    I still need your help for me to find the amplifier direction.
    According to your calculation result and our product have BOM cost limited
    1. what is the parameter of 6.28 ? where can look up the value of OPA172? (Xc=1/(6.28*2.2uF*1kHz)= 72 ohms.)
    2. If the design SPEC need 2Vp-p@32 ohm, operation voltage only can supply +5V, how can we find the suitable amplifier P/N? By what kind of parameter of TI selection guide?

    Thank you very much.

    Vader
  • In reply to Vader chen:

    Hi Kai,
    To correct SPEC is 2Vrms@32ohm.

    Vader
  • In reply to Vader chen:

    Hi Vader,

    Your topic was starting to separate from the original post so I split your question into its own thread. It would be helpful if you could provide a clear post detailing your questions. What are your design goals and specifications?

    Thank you,
    Paul

  • In reply to Paul Goedeke:

    Hi Vader,

    I hope that you have found your questions suitably answered. If you have no further questions, please click the Green "Resolved" button and we will close the thread.

    Thanks!
    Paul

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.