Hi,
Since the OPA875 is a dual power supply, is there a single-supply circuit application for reference?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Since the OPA875 is a dual power supply, is there a single-supply circuit application for reference?
Thanks
Hi Mars,
I think the OPA875 can be used for single supply as well if you connect the +VS to the single positive supply and -VS to the GND. All the logic pins are referenced with respect to GND.
Are you planning to AC or DC couple at the input? If you are AC coupling the input, then you can use the below single supply circuit. For input DC coupling, you simply need to have a 75-ohm resistor to mid-supply or (+VS/2).
Best Regards,
Rohit
Hi Rohit,
Thank you for your reply.
If I need to input the VIDEO (CVBS) signal, is the 75 ohm resistor connected to GND?
For a single power connection does not see in the Datasheet, whether it can provide reference in other documents?
One more, can input ±6.5v (13v) voltage at +VS?
Thank you.
Hi Rohit,
You are correct, my application is the battery of the connector car, so the power supply may exceed 12v, do you have suggestions on the circuit? How to limit the power to 12v, thank you.