Hi team,
The customer would like to select an op amp and need us to provide an available circuit.
His requirements are as below:
1. The input signal is the 1mV amplitude wiht 2MHZ sine.
2. He would like to use single power supply.
3. He need to amplify 2000~3000 times.
4. The output voltage should be 0~3.3V. The output signal is used as the input signal of ADC.
I think this should use the double power supply.
Would you help me to select a suitable op amp and send me a TINA circuit?
The attach is a TINA circuit for this application. Can anyone check it?High gain.TSC
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments