Hello!
i have a question, if the DRV401 is in normal operation,and the measured current is 250A, now, i set the Demag pin to high at least 25.6 μs to start a Demag cicle. in this situation, the probe circuit will still work normally? and the compensation circuit will still work normally? in other words, in this situation, DRV401 will still work normally?why? and is there any negtive influence or harmful toDRV401?
if i set the Demag cicle start every 1minutes when the DRV401 is in normal operation ,is ok?
thanks very much! and best regard!
jie qian.