This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UA741: uA741

Part Number: UA741
Other Parts Discussed in Thread: LM13700

How would I create a circuit that outputs the same amplitude regardless of the input amplitude using op amps if possible?

Vin * X = Vout

X = Vout/Vin = 3V/Vin

Vin min = 0.22mV

Vin max = 2V

Gain min = 3/0.022 = 136.4

Gain max = 3/2 = 1.5