Hi,
I am trying to amplify a DDS sine wave generator using the THS3901. The DDS can produces a sine wave from 50kHz to 70MHz with an amplitude of 50mVpp. As a test, I set up the THS3901 as a non-inverting amplifier and tested gains of 1, 2, and 10 using figure 60 as my reference schematic.
I am seeing significant attenuation of the output starting at 30MHz at all gain levels, which gets worse with increasing frequency. There is almost no output above 50MHz. From the datasheet, I was assuming I would be able to use the THS3901 with a gain of 10 to consistently amplify my sine wave generator output over its entire frequency range. Am I missing something?
Thank you,
Ryan Morrison