This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV321A: Release date of LMV321A?

Part Number: LMV321A
Other Parts Discussed in Thread: TLV9064, TLV9002, TLV9061, TLV6741, LMV321

Dear Sir:

               May I to know the release date of LMV321A? Thanks

Best Regard

Jason

  • Hi Jason,

    Thanks for your interest in our part. This device is scheduled for release early October.

    In the meantime, can I interest you in the attached parts with similar performance and specs.

    Device lmv321a tlv9064 tlv9002 tlv9061 tlv6741
    Num Channels 1 4 2 1 1
    VCC min (V) 2.5 1.8 1.8 1.8 2.25
    VCC max (V) 5.5 5.5 5.5 5.5 5.5
    Iq 25C max (mA) 0.15 0.8 0.075 0.8 1.1
    GBW/BW (MHz) 1 10 1 10 10
    Slew Rate (V/us) 1.7 5 2 5 4.75
    Vnoise (nV/√Hz) 33 11 27 11 3.7
    RR In No R-R R-R R-R
    RR Out R-R R-R R-R R-R R-R
    Ibias (typ) (nA) 0.01 0.0005 0.005 0.0005 0.01
    Vos (Max) (mV) 5 2 2 2 1
    Vos Drift (uV/C) 1 2 0.6 2 0.35

    Thanks.

    Regards,

    -Mamadou

  • Additionally,

    Can you you tell me about your design and how you plan on using this part?

    Regards,

    -Mamadou
  • Dear Sir:

                    Sorry for reply late. We used LMV321A for general voltage amplifier on IoT application. Our customer also used LMV321 but they don't need high voltage supply for OP. Then Supply voltage of LMV321A is 5V. It more  suitable for our application. BTW ,  You mentioned above OP table , It have low ib suitable sensor application? right?

    Best Regard

    Jason

  • Hi Jason,

    LMV321A could be a good option but TLV9061 has even lower bias current if it's one of their main key concern.

    Regards,

    -Mamadou