This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] What are the best cross reference replacement for the MCP6001, MCP6002, and MCP6004 devices?

Guru 52800 points

Replies: 1

Views: 2846

Hello,

 

I need to identify replacement op amps for the MCP6001, MCP6002, and MCP6004 devices.  What are the best replacement amplifiers from TI?

 

Thanks!

Regards,
Collin Wells
Precision ADC Applications

  • Hello Collin!

    Consider the TLV9001, TLV9002, or TLV9004 for 1MHz designs or if higher bandwidths are required consider the TLV9061, TLV9062, or TLV9064 with 10MHz gain bandwidth.

    Here are the latest cost-optimized amplifiers with operating voltages between 1.8V and 5.5V:

    www.ti.com/.../products.html

    Regards,

    Pete Semig

    Applications Manager, General Purpose Amplifiers

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.