This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA857EVM-978: No output from board in photodiode mode.

Part Number: OPA857EVM-978
Other Parts Discussed in Thread: OPA857

Hello;

I have purchased OPA857 EVM for transimpedance amplifier circuit measurement and avalanche Photodiode pulse measurement for my P.h.D thesis.

First I have connected J4 (And I limit the current but when I connect J4 its trying to draw more current each time)  for +VS=3.3v to Test_in input. After I put it in the APD mode. 20K gain. 5 V through the APD Bias Voltage. When I cover the photodiode I have measured the voltage differences  R6 AND R7 independently but There is no voltage change in the R8 that I can measure. and the Resistance seem like 0 ohm on that resistor. And also I can not take any voltage change across the transformer. I Have measured almost every part. I can only find 2 different things R8 seems like 0 Ohm and Reference voltage sometimes can be quite faulty when I limit the current(Because I am afraid it can burn the opamp thats why I limit it to 50ma). 

My application is I will make some very fast pulses from LED and try to measure it through the EVM but I couldn't do it.

Could you please help me with it3

Thanks in advance.

Best regards.