This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM6171: Can high-speed op amp based integrato be paralled to enhance the output capabilty

Part Number: LM6171

Dear TI experts,

Simple question: I’ve used LM6171 as a non-inverting integrator and its output is buffered by parallel connection of several push-pulls as Fig1. In my experiment, the waveforms of G2 follows G1 very well(Their rise rate is about 100V-250V per us). But I soon test the iB1 and iB2 in Fig1 and find the currents is big, and they sum up to around 150mA, which is the output limit for LM6171.

Fig1

My question is can I parallel 2 integrators to enhance its output capability as Fig2? Of course, both integrators’ resistors and capacitors are the same.

Fig2

Best regards