Other Parts Discussed in Thread: INA194, INA193
I am using the INA195 to sense current through an inductive load on the low-side of the load. I have implemented a high-side and low-side switching scheme (essentially an H-bridge) to enable the load. When both the high-side and low-side MOSFETs are not conducting I am seeing variation in the output voltage anywhere from a few millivolts to over a hundred millivolts. Is this type of behavior expected? We are sensing the load over a 0.1ohm resistor.