Other Parts Discussed in Thread: INA826,
Dear All,
I have an output drift problem while evaluating INA826 with TAL220B 5kG load cell. After power is applied, the output reading is correct. However, shortly after it starts drifting to 0 rail and within minutes becomes 0.
Here is my setup:
TAL220B is a Wheatstone bridge with 1k resistors.
A 49.9 Ohm resistor sets Gain to 1000. High gain is needed because load cell produces output in single digit mV range.
I am using a 10V DC rail to power both INA826 and the bridge.
Vref to INA826 is set to 5.6V
Interestingly enough – even though the supply is a single rail, when load is removed, the output signal changes to negative value. When this negative value is subtracted from positive drifting down output, the result is equal to initial output reading at power up.
I am at loss and would very much appreciate help.
Thanks in advance!