This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6518: Will LMH6518 accept differential input?

Part Number: LMH6518

In the datasheet, it says:

The input is differential but is driven single-ended as long as the conditions of Table 6 are met, and there is good
matching between the driven and undriven inputs from DC to the highest frequency of interest.

I'm a little confused, is it mean "although the input is differential, but it can ONLY be driven signle-ended" or "although the input is differential, but it can ALSO be driven singled-ended"? I must make sure this, because I'm considering put another full differential amp before it.

Thanks.

  • Hi,

    your phrase can be found in section 8.2.1.2.2 and is referring to the application shown in section 8.2. But in section 7.3.1 the following is mentioned:

    "7.3.1 Input Preamplifier

    The LMH6518 has a fully differential preamplifier which has a consistent 150-kΩ impedance across all gain
    settings. The LMH6518 is also driven with a single-ended signal source. The preamplifier has two gain settings.
    See Input and Output Considerations for details."

    Kai

  • A single ended signal is technically differential with respect to ground. So ALSO.
  • Hi Sean,

    hmm, the original poster is right somehow. The datasheet is indeed confusing in this point because it only discusses the connection of a single ended signal. Even the eval board is only supporting this configuration.

    Kai

  • Hi Kai,

    You are right as always Kai. There are no examples in the datasheet showing differential input either, and all the specifications are for "single ended input drive". I don't see anything preventing a fully differential input however, other than a lack of examples. Do you have concerns?

    Best regards,

    Sean