Hi,
A customer of mine has some questions about it's behavior. They are trying to change the status of the output alert at a current of 0.5mA and reference of 0.5V.
Normally there should be a current of 5mA (10mA max), with 5V (10V max) at the output of the opamp VOUT, but the opamp is only fed with 3.0V of supply. So the output is clipping.
What are the disadvantages? Is there any recovery behavior? Are there any unexpected effects?
Or is it important to never led the output clip, e.g. at INA381A1 (gain 20) and reference 100mV?
Thank you in advance for looking at this!