Other Parts Discussed in Thread: LM239, , LM2907-N
Weird issue w/LM2917, and I'm stumped.
Used data sheet application circuit because it fit exactly what I was looking for.
Input of 2917 buffered with LM239 comparator, output is into LM285 opamp, with 10K to ground.
Good assembly/solder practices, anti-ESD measure in place.
Vcc is 15V
Works exactly as expected in breadboard, and on 6 of 16 assemblies.
The other 10? No output.
Replace LM2917's? Maybe 1 will work, replace again... Maybe another 1 will work.
Take LM2917 from an assembly that works and swap around to the non-working boards, and they work fine.
If I keep replacing LM2917's, I eventually get 100% operational assemblies.
But that's a lot of LM2917's!
*It pretty much HAS to be something dumb*, but I've scoured the data sheets, and every application anything that I can find.
I played with values, added additional decoupling to the circuit, and so on but didn't seem to make any difference.
Any thoughts or suggestions appreciated - I've never run into quite this issue before!
-K-