Hi
OPA2209AIDGKR is used.
customer's circuit is as below, which is used to sample LLC output 12V power rail current.
the power for OPA2209 is 12V comes from auxiliary power.
when AC power is plug in, auxiliary power flyback works, so 12V for OPA2209 VCC comes out, at this time, LLC is still kept turning off.
12V_Current is connected to DSP ADC pin.
in this condition, customer can see 0.6V at Pin5 and Pin6 of OPA2209, and +12V and +12VX is 0.3V.
after removing R282 and R283, customer can see 1V at Pin5 and Pin6 of OPA2209.
customer want to know why this is no input signal, but input pin has voltage?
thanks.