I design a narrow band pass filter using filter pro. I have selected the Multifeedback single ended, chebyshev filter, with order 8, stages 4 gain of 1.121 V/V central frequency fc at 2250 Hz, band width 50Hz. Kindly suggest me best Opamp for this design. Also as i used the single ended 10 stage opamp (OPA37E) based amplifier before this filtering stage so do i need to select single ended multi feedback amplifier or i can go with fully differential as like ( @TIDA-01036 High-Q Active Differential Band-Pass Filter Reference Design for Instrumentation Qualification). My design is attached kindly check in the attachment.