This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 145
Part Number: LM239
Hello,
Our customer has been using LM239 at high ambient temperature EE.
Recently Tj(max) specification is changed from 105degC to 85degC in SLCS006U datasheet.
They care about offset(max) value which was 15mV over Full range, it was -25 to 105degC.
But now, offset is 15mV at -25 to 85degC, seems de-graded offset performance very much.
Is this true understanding that “new production lot” device has larger offset than previous device at 85degC?
Or, actually offset performance is same as “previous lot” device but just changed Tj(max) specification on datasheet?
Regards,
Mochizuki
Paul Grohe
TI Comparators (CMPS) Applications Group
In reply to Paul Grohe:
Hi Paul-san,
Thank you for your prompt reply.
Okay, this correction is just in "front page" section , not in "Recommended operating condition" section.
Then it is clear that no change of actual device performance.
So, we should not heat up about this subject even it is simple and confusing typo :-)
In reply to Mochi:
In reply to Chuck Sins:
Paul-san,
Thank you for your support.
We will visit our customer this week to explain this fact.