This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV6710: TLV6710

Part Number: TLV6710

Good morning, I would like to use TLV6710 as window comparator in order to detect undervoltage and overvoltage on a 24V voltage supply. Undervoltage must be set at 19V and overvoltage at 36V.

I would like to supply the comparator with the same monitored 24V voltage supply and also the pull-up directly connected to 24V voltage supply. The problem is that in the datasheet the maximum pull-up is 25V whereas I could have 36V .. But I have to optoisolate the comprator output so at the output the possibility is to have 0V (comparator pulls down the output) or 1.1V (when the comparator gives high impedance the optoisolator is ON).

Is it possible for me to use this configuration and pull-up of 36V?

Thank you.

Attached my circuit configuration