This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 7
Views: 257
Part Number: OPA2348
Hi
Our customer has question about OPA2348.
I attach the circuit below with simplified.
2476.e2e.xlsx
Two OPA2348 are tested in same circuit.
Device A : 100mV at Probe_X and 100mV at Probe_Y.
Device B : Nearly 0V in both Probe point.
1.
OPA2348 offers voltage output swing from fail in electrical characteristics.
(25mV when RL=100K, A >94dB and 125mV when RL=5K, A > 90dB)
Should this voltage appear at output when the input is not applied?
2.
In this time, Device A and B show different result.
Could it be possible result?
The customer uses OPA2348 for current sensing, so they want to avoid such variation because it leads to measurement error.
BestRegards
In reply to Paul Goedeke:
In reply to na na78:
Hi Paul Thank you for your reply. So, in the following two cases, I added my understanding. Could you please review? Device A : 100mV at Probe_X and 100mV at Probe_Y. -> If the offset voltage of two opamp are called Vos1 and Vos2 conveniently, Vos1 at first stage opamp is increase with gain of 44 and it appears at second stage opamp. Basically, we can not say that Vos1 and Vos2 are equal. Device B : Nearly 0V in both Probe point. -> In this case, it can be considered that Vos1 x 44 is smaller than output swing limit (VEE+25mV). It can be considered that ~25mV (or output swing limit) appear at output. Is my understanding correct? BestRegards