This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR106: know the XTR106 was damaged or work correctly

Part Number: XTR106

is it any way for test of XTR106?

I give constant 1V between pin5 and  Pin2 and I put ampere meter between pin2 and pin3 of P1 connector but the current was zero! is it mean the XTR106 was damaged?

and the voltage between pin14,pin11,pin6 and ground (pin2 of P1 connector) is near Vcc=24V!!!