Other Parts Discussed in Thread: INA139, LMP8645HV, , LMP8640, INA137, INA592
Hi team,
I received the following request.
Could you, please, suggest the correct device/reference designs for this application?
###################################################################
I am working on an a digital DC-DC application below 48V. For the feedback loop I am looking for a convenient IC, to sense a 2mohm-3mohm resistor up to 20A. The effective frequency might be as high as 1MHz, but ideally 800kHz.
The question is the product with the highest bandwidth is INA1x9 series which has 4400kHz bandwidth.
However, the gain for high bandwidth applications is too low, therefore an amplifier will be necessary after the shunt IC which could add errors to the feedback. Plus in the datasheet 0dB gain is not constant over 400kHz for this series of ICs. See below:
I would like to control the peak current, therefore accurate sensing is necessary, delays on the feedback loop should be minimized. What is the correct product for sensing the current accurately for an application up to 1MHz? Is there any other differential amplifier product available for my application. Please note that the input of the monitoring should stand 48V.
###################################################################
Regards,
Fabio