This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LM318-N: input voltage range for single power supply

Mastermind 6180 points

Replies: 1

Views: 109

Part Number: LM318-N

Hi,

LM318-N's maximum voltage is +-20,  and input voltage is +-15V.

So can it support single power supply to +40V and +30V input?

Thank you.

C.T.

  • Hi CT

    Yes, the device can use a single +40V supply. The input voltage needs to be at least 5V above VEE and 5V below VCC, so for a single supply +40V, the input voltage needs to be above 5V and below 35V.

    I hope that is clear,
    Paul

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.