This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA5807A: LNA solution

Part Number: PGA5807A

Dear E2E,

Do we have LNA solution which spec is shown in below?

Operating Frequency 734 ~ 960MHz

Gain 13 dB

NF 1.1 dB

Supply voltage 1.5~3.3V     2.8V (typ.)

BR,

Jason