Other Parts Discussed in Thread: AMC1301, AMC1302
My customer raised 2 questions regarding AMC1302-Q1 to me.
1. Connection between GND and INP allowed?
It says on page 25 in the datasheet: "The floating ground reference (GND1) is derived from the end of the shunt,resistor, which is connected to the negative input (INN) of the device." That would mean TI indicates a need of GND1 and INN to be connected at all times. In Figure 56 the current is positive to load, which would mean that there is a negative differential input voltage between INN and INP and therefore would create a negative differential output voltage between OUTP and OUTN. The customer plans to have a positive current to load (similar to Figure 56) but result in positive differential output voltage instead. They want to connect INN behind R_shunt and INP before R_shunt. Then INP and GND1 would be connected which per datasheet does not seem to be a viable option. Could you let me know if that is really the case and if so why can INN only be connected to GND1 and not INP?
2. Output voltage on AMC130xEVM centered on VDD2?
In the user manual of the AMC130xEVM it says in 4.3 " The output voltage of the AMC130xEVM is centered on VDD/2 and..." That would mean in case VDD2 =3.3V the center of the output voltage would be 1.65 V, with VDD2=5V the center of the output voltage would be at 2.5V. Based on the datasheet of AMC1302-Q1 Figure 37 the center of the output voltage is always at 1.44 V which would be independent of VDD2. Could you comment?
Thank you in advance and kind regards,
Sally