This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2890: Some further BP active filter testing the DABP topology

Part Number: OPA2890

Before I leave this newer (to me) BP filter topology, I stepped through a more demanding design targeting total 6dB gain with 1MHz center and only 50kHz BW forcing a 4th order solution in Filterpro. It does not support this topology, but using a MFB, it asks for > 1.5GHz GBP for the Q of 18 in each stage. That is too high a Q for MFB designs - and, while a mixture of computation and iterative R adjustments got the nominal design pretty close with the DABP approach, the response spreads are actually pretty high even using 1% C and 0.5% R. The implementaiton with a much slower (130MHz GBP) is pretty close nominally so it is possible to use a much slower device here than Filterpro suggests, but it would be interesting to test the shift to some GBP spread in the model - later. 

5557.4th order BP using the DABP topology.docx

4th order DABP with OPA2890 2stages.TSC