This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA237: ESD LEVEL & TEST SPECIFICATION

Part Number: OPA237

We are updating our component information and are in need of the following information:

 

ESD LEVEL:

ESD Test Specification:

 

Hope to hear back from you in a timely manner.

  • Hi Dianne,

    As you know, the OPA237 is a really old device so that information is not in the datasheet. Most modern op amps include HMB and CDM ESD tests / specs.

    For the OPA237, the HBM spec is 2000V.

    Would you consider using a newer device? I can help you fine one given the system requirements.

    -Tamara