Other Parts Discussed in Thread: TLV7011, TLV1805
HI Sir: this is my test circuit. When I connect the PIN3 to GND . The output should be Low. But I find that When I power on. there is short high pulse. pls ref the picture. I want to know why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Lei,
Assuming the scope vertical is 1V/Div, it looks like the supply voltage is between 1V and 1.2V with a fairly slow ramp.
As Kai said, the minimum supply voltage is 2.7V, so the device is just becoming awake at 1V, but is not fully biased yet. 1.2V is about where the internal circuitry starts to wake-up but not fully biased. So the output "flops" as the supply votlage ramps up to the minimum supply voltage.
What Kai said is <mostly> true, is that most comparators will glitch as the supply is ramped-up.
HOWEVER, we have now been introducing comparatos with an internal POR circuit that minimizes this power-on "glitch" by requiring both a time and minimum supply voltage limit be met before the output starts responding to the inputs.
Please see the TLV7011 or TLV1805 family of comparators. The fastest is 250ns, hopefully that is fast enough for you. The supply votlage must cross 1.6V and/or power must be applied for 20us. The output will be low during this time.