This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7171: 20v output amplication

Part Number: LM7171

Will the output of this circuit be 20v ? The input Sync_vid_1 is 0 to 3.3v unipolar input coming from FPGA. 

  • Hello Ashish,

    I would give R85 a value, say 1kohm to make sure the V+ input sees a path for Ibias.

    The gain is set to 6 you will get a 19.8V output.

    Why are you showing R84 as a shunt termination - if you are driving a 75ohm transmission line it needs to be where R83 is and eliminate a resistor to ground. Of course if you are terminating the cable in 75ohm you will get a divide by 2 on that 19.8 at the end of the cable.