Other Parts Discussed in Thread: DRV134, DRV135, DRV632, DRV603
Hi,
Greetings !!
Need help to understand how effective the below scheme is for converting single ended signal to differential and transmitting the same on a shielded, twisted pair for a distance of 25 mts. ( The scheme is suggested by a TI employee and has asked me to get it reviewed as he is not well-versed with INA 826)
Requirements
1) signal is a pulse in the range of 250 mV to 4.5 V and frequency ranges from 1 KHZ to 9 KHz .
2) media of transmission : 25 mts.shielded, twisted pair
2) For my application I prefer to use dual supply opamp (+/-5V)
3) ESD and Noise protections are necessary
4)) what is the error in the amplitude I can expect ( is it within 2 to 3%) ?
5) How do I arrive at the % error in amplitude ?
Regards