This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TL082: Poerr supply

Prodigy 40 points

Replies: 2

Views: 122

Part Number: TL082

Can TL082 be powered by single voltage supply,such as +12V without -12V?
  • Yes, this is possible. But keep in mind that the common mode input voltage must stay 4V away from the supply rails and that the output cannot reach the supply rails. Or, by other words, the TL082 is no rail-to-rail OPAmp. Have a look into the datasheet.

    Kai
  • In reply to kai klaas69:

    User,

    Yes, TL082 can be used if Kai's advice is followed. For wider input range with similar performance and 1k/u web price, consider TL3472 or TLV2172 instead.

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.