Hi Team
My customer would like to grasp min AGC range but there is no specification
in datasheet.
Could you inform the characterization data if you have even it is not guaranteed.
Thanks
Best regards
Shidara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Shidara-san,
The maximum gain is variable in the specification and typical chart. When it is lowest that also shrinks dAVD, including temperature [typical down to min] is [85V/V down to 55V/V], that loses 4dB. I don't have much insight to the minimum attenuation and there is no specification for that. My best guess is that 6dB should cover it. That makes 40dB as a minimum delta, but I can't be certain.