This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL074A: Load Resistance = 100K Ohm

Part Number: TL074A
Other Parts Discussed in Thread: TL074, TL082

Hello, In the SPEC of the Figure 6. Maximum Peak Output Voltage vs Load Resistance, it shows the VOM vs. RL.

However, the max. RL is 10K Ohm. What happens if the RL goes up to 100K Ohm? Very thanks. 

Application: Industrial Motor

Regards

Brian Wang

  • Brian,

    Almost nothing happens. As the curve approaches 10k it is flattening out. Going to 100k and beyond, the curve continues to flatten. 100k only gains a little voltage that would be hard to see on figure 6 chart.

    Here is TL082 at +/-5V chart where it is easier to see voltage and gets closer to 100k. This chart also separates VOL and VOH. The lower supply voltage makes lower load current which emulates  a higher resistance at +/-15V. TL074 will be similar to this.

    Do you need a low cost rail to rail output alternative?