Other Parts Discussed in Thread: OPA192
Hi, all
I have proposed an OPA2192 to kick out ADI's OPAMP.
One application is a driver for the 250ksps SAR ADC and the other is a REF driver. I thought that the superior DC and AC performance of the OPA2192 could be used for both purposes.
The customer's circuit needs to invert the signal for the ADC driver. Although the settling by the step response was verified by TINA at Rf = 10k and Rg = 10k, a slight ringing can be seen at 10k.
DS uses 1k. It was very clean when I checked by TINA.
Question: Does TI not recommend Rf = 10k?
For customer applications, 10k is the best choice due to current consumption and input impedance.
The ringing was corrected when Cf = 10 pF was used as a countermeasure.
Is this solution correct?
Please tell me if there is a value confirmed by measurement by TI.
I think 2-10pF is reasonable, but I need to complete the circuit design immediately for ADI kickout.
(*I connected a 15pF load capacitance to the output pin, TINA seems to have almost no impact.)
//Rf = 10k
//Rf = 10k with 10pF
Rf = 1k without Cf
Best regards,
Hiroshi