Hi Team,
I want to realize the system such a shunt solution using AMC1301.
Is it possible to output analog signal from 0.5 to 4V when the current which through the shunt resistor is from -2000A to 2000A?
In my understanding, If I can use 125uOhm for shunt resistor, I can realize the system such an above mentioned. Is it correct?
If so, could you have the wave form which is like figure 24. when the VDD2 is 5 V.
Thanks,