Other Parts Discussed in Thread: , TLV2314, TLV9002
Dear all:
Our company USES TI LMV358 to form a voltage follower circuit (see attachment), and USES 3.3V for power supply. When the input of 0-3V varies linearly at the same phase end, the output follows 0-3V.
The test results are as follows:
When the in-phase input is less than 2.7V, the voltage follows well. When the in-phase input is more than 2.7V, the abnormal results are as follows:
1. The output terminal voltage jumps to 3.276V (same as the measured supply voltage 3.276V)
2. The output terminal voltage is fixed at 2.726v (the actual supply voltage is 3.276V)
When the output is abnormal, the input terminal voltage still changes linearly accurately, so the LMV358 output is abnormal.
May I ask the following questions: 1. What is the input voltage range of LMV358?Whether input above 2.7v in the same phase will cause it to exceed the linear workspace
2. What is the output voltage of LMV358 beyond the linear working area?
3. What is the input range (curve) of different supply voltage?