Other Parts Discussed in Thread: OPA188, OPA189, THS4001
Hi,
I am using TLC2652 in a composite circuit wherein the Cxa and Cxb are connected to VDD- as per datasheet.
The circuit is as shown below.
I am observing the output to be -2.5V with -5V input voltage with the Cxa and Cxb connected to VDD-.
But i am able to get the output as 2V if the Cxa and Cxb are grounded.
Need suggestions for the same.
Thanks
Pavithra Joshi