This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Original question:
LMV339 VICR common -mode input range
Replies: 1
Views: 68
Part Number: LM2903-Q1
Dear expert:
I have similar question. According to parameter Vicr and note3 of 6.6 EC table, can I draw conclusions listed below? Could you kindly correct me please?
1. common mode input voltage range is "0 to vcc-2v" at full range?
2. non-inverting input range is "-0.3v to vcc"?
3. what is inverting input range?
Thanks a lot!
Hello Lin,
These questions are answered in the appnote provided in the other post.
Both inputs have the same limits. You must consider each input individually, so *each* input has the -0.3V to (Vcc-2V) limit.I will close this thread as it is close to the other thread. Please reply to the other thread.
Regards,
Paul Grohe
TI Comparators (CMPS) Applications Group