Other Parts Discussed in Thread: TLV2462
One of my customer is using TLV2462 rail-rail op amp for pressure sensing application in our product. As per datasheet if capacitive load more than 10pf then suggested to use min 20ohm resistor in series, what will be the maximum capacitive load that op amp can drive without degrading performance?. Initially they used 1K resistor in series for 0.1uf capacitive load but at some point of time op amp output limited around 3.5V even though change in input voltage. They tried tweaking resistor value for proper response and then we got expected results with resistor <470ohm(Finally used 100ohm and 0.1uf). Please let us know the op amp response here with high value resistor.