Hello, I am planning on using the INA260AIPWR PWR/Current Monitor in my next design. I want to know that max current the device can handle through pins IN+ to IN- would that be the "Maximum Continuous Current" found on page 6 under the Integrated Shunt heading? That spec is +15A and -15A. I need to be able to handle 40A could you suggest a device if this one can't handle that current?
Thanks,
Joe