Other Parts Discussed in Thread: LM124, LM124-N
I’m using the LM124A in a static condition as a voltage follower and have a couple application questions. First, if I am biasing at +5/-5V, what is the max positive output voltage that it will go if it attempts to rail to the positive supply? I cannot go over 3.3V output under any condition.
Second, I am biasing it with +5/-5V. Due to power supply sequencing that I cannot control, I will be applying up to -1.5V to the non-inverting input prior both to the +5 and -5 volts coming up. The approximate timing is -1V applied at Time=0. The +5V comes up ~40 mS later and the -5V comes up 40 mS after the +5V. What will the output do during the power supply bring-up when -1V is applied to the input with no bias and then only +5V bias? Will the output go to 0V with only +5V turned on?
lastly, I’m using this as a voltage follower to provide a DC low impedance steady state. It won’t be switched or changing amplitude so frequency is not an issue. I am questioning the follower in terms of any potential oscillations, do you have any cause for concern using the LM124A?