Is there any way for end customers to interpret the lot and/or date code marking an the Op-Amp OPA602AU?
Examples: 892GQ, 6BQ5J, 68Q5H (the "8" is posibly a "B" => 6BQ5H)
The same challange with TL062AC; examples: 75M ALCP, 75M ALCQ,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any way for end customers to interpret the lot and/or date code marking an the Op-Amp OPA602AU?
Examples: 892GQ, 6BQ5J, 68Q5H (the "8" is posibly a "B" => 6BQ5H)
The same challange with TL062AC; examples: 75M ALCP, 75M ALCQ,
Hi Peter,
TI is unable to provide lot/date code product marking information on the e2e forum. The problem is if we reveal our product codes on the open forum counterfeiters can use the information to mark their counterfeit product making them appear more legitimate and less easy to detect.
If you obtained your OPA602AU and TL062AC product directly from TI, or a TI authorized distributor, it should be valid product. The Date code (work week) is provided on the shipping label attached to the original TI shipping medium. If you can't identify the date code information on the shipping label, then an image of the shipping label should allow us to identify it for you.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas,
the story is much complicated than it seems. The first: On this issue, I work for Thermo Fisher Scientific. Since more than two months one of the suppliers (Scanfil) has serious technical problems with a series production of one of key boards.
I understand that this is not the right place to discuss this. ;o)
Please provide a contact person to me. I would like to provide more details.
The key information: While searching for the reason of the technical problems I found out that Op-Amps OPA602AU seem to show something like “pop corn” effects. This happens sometimes only once within 12 hours sometimes five, to ten times. This only occurs with the Op-Amps with the lot/date code 892GK or 892GS.
Ok... I think this should be enough information here... ;o)
Kind regards from Germany,
Peter
Hi Peter,
Send me a "friend" request here on the e2e. Once we have that set up we can exchange email information. I am not sure exactly what I am allowed to reveal regarding the code information, but I will try help if permitted.
Do you have any possible way of determining which decade the OPA602 devices were put into service?
Regards, Thomas
Precision Amplifiers Applications Engineering