This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4520: Using THS4520 to do a Fully differential op amps as an attenuator

Part Number: THS4520
Other Parts Discussed in Thread: TINA-TI,

Hello,

I read a lecture of Jim Karki's  'Using fully differential op amps as  attenuators, Part 2: Single-ended bipolar input signals'.FDA as atten_Part2_SEB.pdf

And I use TINA-TI to do simulate.

Here is my requirement:

1. Input: Single-end.

2. Input impedence = 1M ohm.

3. To attenuate a signal of Sine wave 50V 1Meg Hz to 250mV 1Meg Hz, which means 250 times attenuation.

Could anyone give me some ideas to implement the simulation by using THS4520?