Other Parts Discussed in Thread: TLV7022, TLV7012
Hi Team,
We are looking in for AC over current sensing application of a 3 phase motor inverter.
Current transducer output is from 0.5V to 4.5V.
Over current threshold limit: 1V (Lower limit) and 4V (Upper limit)
We are able to achieve this using a common dual comparator with TLV1702-Q1. I have attached a basic simulation file as well.
We would like to know the if the below additional requirement can be achieved,
- The comparator must output HIGH, only if the "Vsig" is exceeding it's threshold for 3 cycles (3 x 50Hz = 60ms)
- VOUT must remain HIGH until it gets a reset signal from MCU.
- Also, is it necessary to have R2 and R3 in simulation, because i am not able to simulate without them
Kindly support.
Regards,
Mohana Krishnan MOCP.TSC