Other Parts Discussed in Thread: OPA363, OPA365, OPA810, TLV9002, OPA376, ADS1115
Hello,
I have two questions.
I plan on using the OPA380 as a current-to-voltage converter for a thesis project. The current source is a photodiode that is expected to produce a maximum of 5 uA. It has a capacitance of 5 pF and is recommended to be reverse biased at 5V per its datasheet.
I was planning on creating the following schematic where Vcc is 5V, PD_C is the photodiode cathode, and PD_A is the photodiode anode. The resistor is chosen as 1 meg to provide 120 db of gain. 1) I'm worried about biasing the OPA380 input at the power supply voltage. Should i be concerned here? Is says in the datasheet that the input voltage can tolerate Vcc+0.5 but I'd like to be safe and ask first. I know pushing the limits can cause weird edge cases sometimes.
2) Is the OPA380 still the preferred method of a photodiode transimpedance amplifier? A digikey reference design uses a more general purpose amplifier that actually has a lower offset voltage, the OPA363. https://www.digikey.com/en/articles/techzone/2017/jun/how-to-design-stable-transimpedance-amplifiers-automotive-medical-systems
Thanks,
Mike