The datasheet seems to have some conflicting information for the OPA548. In the electrical characteristics it lists the specified range as -40 to 85C, but in the recommended operating conditions it lists the specified temperature at -40 to 125C. I saw there was a similar question earlier, but this seems to be an error in the datasheet. Which temperature range is this specified over? My main concern is if I run the part at a junction temp between 85 and 125C, could the part not meet parameters specified in the electrical characteristics? Do I need to keep the junction below 85C to get the published datasheet electrical characteristics?