This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TLV2371: TLV2371 ESD HBM/CDM/MM data

Expert 1525 points

Replies: 1

Views: 38

Part Number: TLV2371

Hi Sir


Could you help to share ESD HBM/CD/MM data? Since I can't find it in spec.

Thanks for your great support.

  • Hugo,

    There is no data sheet rating for TLV2371. I did find ESD sample data for TLV2370, dated 3/15/2001. TLV2370 is a TLV2371 except it has an extra pin for shutdown. HBM was tested up to 4kV and passed (2kV was the highest test voltage for other TLV237x part variant jobs). MM passed up to 300V. CDM passed up to 750V , but wasn't tested higher. The quad was tested up to 1500V and passed. This is sample data and not a data sheet rating.

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.