So I'm trying to pick out the proper dual channel SOIC 8 op amp to use as a current sense amplifier. I understand how to set up the op amp to achieve this but I have questions concerning the properties of the op amp.
1. How do I determine what bandwidth is needed? The control loop speed of my application is about 30kHz. Switching frequency can be up to 40kHz. The gain for the amplifier will be 20 so I know this reduces the BW of the op amount by a division of 20. Does this mean the op amp should be at least 30kHz x 20?
2. How do I determine the slew rate? I see this specification often as one of the headlining properties of an op amp. I know what slew rate is but I'm not sure of its significance to my application.