Other Parts Discussed in Thread: TINA-TI, OPA828
Dear all,
I would like to ask a question about output voltage range.
When the output voltage range of the OPA627 was confirmed, only the case where the power supply voltage was ± 15 V was described as follows.
Our customers are going to use with output voltage 5V.
At this time, what is the output voltage if the measurement conditions are the same as the above figure?
I believe that when the power supply voltage is 5V, the output voltage min will be ± 1V.
Best Regards,
Y.Ottey