Hello Team,
in the datasheet it is written that the INA381 may withstand higher Vcm in case the current on the inputs is limited by 5mA max.
On the PCB we have already the filter resistors on IN+ and IN- as in the datasheet section 8.1.4, that can be used to limit the current.
30V is not a normal working condition, but a fault condition. If this will happen, the INA381must not get broken as well.
I would assume that if Vcm is 30V the fault current is 30/Rin+ < 5mA thus Rin+ must be > 6K.
- Does the internal INA381 input stage allow to use the flowing formula (30V - 26V)/R instead?
6K on the input is quite high, the tolerance on that will create an error (which is fine).
- What is the input impedance of the INA381?
Thanks,
SunSet